6/16/2010 6:58 PM | |
Posts: 18 Rating: (6) |
why it is notpossible to run two identical motor with the help of single drive in vector control mode? |
6/16/2010 8:07 PM | |
Joined: 9/27/2006 Last visit: 5/12/2024 Posts: 12257 Rating: (2667) |
Hello manoj; I remember reaserching this issue a while back, when we were discussing multi-motor apllications with MM440s. The following FAQ was interesting: Applying Sensorless Vector Control (SLVC) http://support.automation.siemens.com/WW/view/en/7494205
|
Follow us on