12/28/2007 9:09 PM | |
Joined: 1/7/2006 Last visit: 11/17/2023 Posts: 2705 Rating: (315) |
Dear Forum, I have tested on a FieldPG M with VISTA Ultimate (I have all updates done) with STEP7. The software that is placed here is tested and given free for the two versions of VISTA that are mentioned here: MS Windows VISTA 32 Business and Ultimate. Also the FORUM is VISTA-proof, tested by me, however nobody have say that it works, I could do everything that I want. The next software is given free for VISTA: STEP7 V5.4 SP3.1 Service Pack 3.1 for STEP 7 V5.4 and STEP 7 Professional Edition 2006 PLCSIM V5.4 Service Pack 1 for S7-PLCSIM V5.4 S7-GRAPH V5.3 SP4 Service Pack 4 for S7-GRAPH V5.3 S7-SCL V5.3 SP3 (SP4 coming soon, some errors by compiling in SP3) Service Pack 3 for S7-SCL V5.3 and STEP 7 Professional Edition 2006 S7-200 Microwin V4.0SP6 STEP 7-Micro WIN V4.0 Service Pack (SP6) Download SIMATIC NET 2007 SIMATIC NET PC Software Products Edition 2007 based on the SIMATIC NET CD 2007 is released for delivery Distributed Safety V5.4 SP4 S7-Distributed Safety V5.4 + Service Pack 4 Also the FM352/452 package is given free for upgrading to VISTA Configuration Package for Cam Control FM 352 FM 452 V6.0 And SINEMA E is now also given free with version SINEMA E 2006 SP2 Service Pack 2 for SINEMA E 2006 Available for Downloading ET 200S 1SI Serial Interface Function Blocks, Examples and User Manuals for the ET200S 1SI Serial Interface --- new from February 2008 Loadable driver CP PtP DataHighway (DF1) Configuration Software for FM 355-2 Temperature Control Version 6 SP1 Configuration Package for FM 350-1 and FM 450-1 Counter Modules Version 6 Configuration Package for FM 355 - 455 PID Control Version 6 SP1 Loadable driver CP PtP Modbus Master (RTU) V3.1.4 Loadable driver Modbus Slave (RTU) V3.1.5 ----- New from march/april 2008 ---- The package for the FM352-5 High Speed Boolean Processor is given also free for VISTA. The Configuration Package for FM 350-2 Counter Module is also given free for VISTA. ----- New fromjuli 2008 ---- The package for the Configuration Software for FM351-1 Positioning Module is given also free for VISTA. --- Testwork for STEP7 / SCL / S7-GRAPH and PLCSIM I made a small project with some S7-SCL and S7-GRAPH and tested it with PLCSIM, that was working well. After that I switched the option Report System Error on (in the Hardware configuration --> Options --> Report System Error) and I checked that with "CPU Messages" in the "STEP7 Manager". So there where no errors or problems.... I have stillone problem, the drivers of the soundchip, the screen and the CP5611 are not delivered. The wireless connection and the onboard IE port are recognized by VISTA. So I have not yet heared anything of VISTA... --> See INS sugestions that is working fine. |
Last edited by: Late at: 7/8/2008 9:27 AMAdd VISTA versions that are given free Last edited by: Late at: 5/10/2008 2:36 PMAdd VISTA versions that are given free Last edited by: Late at: 4/23/2008 1:55 PMNew packages from march/april 2008 Last edited by: Late at: 22.02.2008 11:11New VISTA packages Last edited by: Late at: 06.01.2008 20:59Last edited by: Late at: 05.01.2008 14:55Postet all links of the different packages so that the visitors of the forum don't have to search for the packages. All the installations are described in this thread. Last edited by: Late at: 28.12.2007 21:11change some text I hope that the answer will help, if you have still questions, don't hesitate to ask me. |
|
12/30/2007 2:36 PM | |
Joined: 4/6/2006 Last visit: 2/5/2024 Posts: 604 Rating: (56) |
Hello Late, There is an Entry-ID about the Audio driver issue on the CS-Site. Maybe it will help to solve this issue. What should you pay attention to when installing Windows Vista Ultimate or Vista Business on the Field PG M? Good luck, I'm curious or this Entry-ID solved it for you. |
Last edited by: INS at: 30.12.2007 14:37Best regards, |
|
Follow us on