2/18/2020 6:21 AM | |
Joined: 1/1/2017 Last visit: 4/22/2024 Posts: 329 Rating: (11) |
Dear Team, I am migrating PCS7 V6.2 SP3 project to PCS7 V9.0 SP1. Hereby are the following steps I've done: PCS7 V6.2 SP3 migrated to PCS7 V7.0 SP3 PCS7 V7.0 SP3 migrated to PCS7 V7.2 SP1 PCS7 V7.2 SP1 migrated to PCS7 V9.0 SP1 Hereby are the errors we are facing: 1. s7omwinx: Opening the project failed. Cannot open or start WinCC project as Project Manager cannot start basic application XREF. 2. After Forum search done some diagnosis and new error came: WinCC Server not available I have attached the list of installed softwares also. Kindly refer the attachement. Please guide me to sort out this issue! Regards OmKris AttachmentVM PCS7 V9.0 Issues.zip (51 Downloads) |
2/19/2020 6:48 AM | |
Joined: 1/1/2017 Last visit: 4/22/2024 Posts: 329 Rating: (11) |
Sorry Team! Solution found. Regards |
This contribution was helpful to1 thankful Users |
Follow us on