8/19/2010 8:01 AM | |
Joined: 3/21/2006 Last visit: 9/10/2024 Posts: 10228 Rating: (1181) |
Hello, Unfortunately, there is no official release for the VNC and PCS7. According to PCS 7 V7.x Kompatibilitätsliste like remote software could use either Symantec pcAnywhere V11.5, either Microsoft Windows NetMeeting. Best regards, Hristo Mihalev |
8/19/2010 8:20 AM | |
Posts: 183 Rating: (8) |
Hello JeffSibley; For V7.1 Itested that doesn't work with Microsoft Remote Desktop and it works with Real VNC. |
9/17/2010 11:31 AM | |
Joined: 5/19/2010 Last visit: 2/7/2024 Posts: 22 Rating: (2) |
Hi JeffSibley, I use UltraVNC (currently on v1.0.8.2) with PCS7 v7,1 and it works pretty well, no conflicts or problems found as yet. Obviously not supported by Siemens (well I've never found anywhere it says it's supported) but in my experience it works well. I find UltraVNC the best of the VNC bunch as it includes a file transfer function which can be very useful. I'm currently using it to program and commission a project from 120 miles away across the internet. Hope this helps Tim |
Follow us on