1/29/2012 5:16 PM | |
Joined: 8/31/2010 Last visit: 9/18/2024 Posts: 1521 Rating: (227) |
Hello Ahmed Mandor, Check the enclosed screenshots on how to insert the VS120 into your Network View. 1. Double Click - Devices and Networks 2. Click on Device View 3. Click on Hardware Catalog 4.Choose the VS120 PROFINET (VS120_PN.jpg) / PROFIBUS (VS120_DP.jpg) variant 5. Check for the right MLFB of the device which you are using Still to download the GSD file for VS120 from here - PROFIBUS GSD-Files: VS120 Find details on - Using GSD files Using GSDML filesin STEP 7 Basic v11 SP2 AttachmentVS120 in STEP 7 v11 SP2.ZIP (328 Downloads) |
Like it? Rate it! |
|
This contribution was helpful to1 thankful Users |
1/29/2012 5:37 PM | |
Posts: 19 Rating: (0) |
thanks Ganes10 |
This contribution was helpful to1 thankful Users |
1/29/2012 5:43 PM | |
Joined: 8/31/2010 Last visit: 9/18/2024 Posts: 1521 Rating: (227) |
You are welcome and it's a pleasure. |
Like it? Rate it! |
|
1/29/2012 5:55 PM | |
Posts: 19 Rating: (0) |
dearganes10 i had configurate it successufly and used profibus in communication. I attached image of network, hope to give me ur comment. thanks.
|
2/24/2012 2:41 PM | |
Joined: 8/31/2010 Last visit: 9/18/2024 Posts: 1521 Rating: (227) |
Hello Ahmed Mandor. Check this new FAQ on "How do you configure the SIMATIC MV440 / MV420 code reader device with STEP 7 BASIC V11 (TIA Portal) as a PROFINET IO device on the PROFINET IO system of a SIMATIC S7-300?" MV440 and MV420 PROFINET configuration can be found here. But I'm surprised on why it is mentioned as STEP 7 Basic when the controller usedin the FAQis S7-300 |
Like it? Rate it! |
|
This contribution was helpful to1 thankful Users |
Follow us on