2/23/2018 1:19 PM | |
Joined: 3/14/2008 Last visit: 4/18/2024 Posts: 2064 Rating: (926)
|
Hi, The warning times could only be set in manual and automatic mode AND when using a "Large" block. |
If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to1 thankful Users |
2/24/2018 11:17 AM | |
Joined: 3/14/2008 Last visit: 4/18/2024 Posts: 2064 Rating: (926)
|
Yes, WarnAct does not work in local mode. You can make a simple function: Give a start signal locally, which you connect to ExtMsg01 to trigger a message (which you can define yourself) and connect to a timerp block, where after a delay time (On-delay), you give the motor the actual start signal. |
Last edited by: Oreca at: 2/24/2018 7:48:55 PMIf I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to1 thankful Users |
2/27/2018 1:52 PM | |
Joined: 5/3/2017 Last visit: 4/19/2024 Posts: 673 Rating: (216) |
Hi tungpt3149, in the manual "Engineering System (V8.0)" under the chaper 6.1.9 you find more information about How to configurate a message under PCS 7 V8.0. Here is the link your the manual And there is more information in post "How to change the Event message on ExternalMsg": With regards |
Last edited by: Heisenberg2 at: 2/27/2018 2:33:00 PM |
|
2/28/2018 7:04 AM | |
Joined: 3/14/2008 Last visit: 4/18/2024 Posts: 2064 Rating: (926)
|
Hi tungpt3149, Check the following thread: Alarm8P for an example I attached in my post. |
If I could help you, you can use the RATE button. Thank you. |
|
Follow us on