7/24/2007 9:27 PM | |
Posts: 1275 Rating: (123)
|
Hi Darius, Some functions, specially in C, aren't compatible with WebNavigator. In Web Navigator online help you can find those function, which are possible with Web Navigator. I have an old list of unsupported functions, so I'm posting it here... you should look in the help either way, just in case... You said you make calculations using scripts. How are these scripts called? When you open a screen, or a command box? Have you made sure that the web navigation isn't getting mixed up with the regular operations (they could be using the same internal tags for calculations, at the same time, for instance). Remember that all scripts are executed in the server, so it's the same script engine for the operating station which is the web server and the web clients... You also said sometimes some tags are updated, and others not.. do those which are updated depend on this function? Have you ran your project under APdiag, to check for any script errors? Also... check this out... It's the Web Navigator v6.2 compatibility list... it only mentions IE 6... Best regards, Danielle AttachmentWebNav - Unsupported Functions.PDF (440 Downloads) |
Last edited by: Danielle at: 24.07.2007 21:36Last edited by: Danielle at: 24.07.2007 21:31 |
|
8/3/2007 6:58 PM | |
Posts: 1275 Rating: (123)
|
Hi Darius, I found this FAQ with Web Navigator 6.2's compatibility... the supported IE version for the Web Client is v6.0 SP1 or 2... Try accessing your server from a station with on of those versions of IE, and see if it works... By the way... after changing your .Pdl's you've published them again, right? Best regards, Danielle |
Follow us on