10/2/2011 1:32 PM | |
Joined: 9/9/2011 Last visit: 4/18/2024 Posts: 102 Rating: (3) |
Hello I have try every exemple of Pegaiaabout webserver and It's working very well ! thanks to him. Now : During production :I would like nowto make a datalog of 1 analog input every secondduring all theproductiontime (around 10 minutes : 600 values ) I would liketo save every datalog with aFIFO of 10 productions files. I would like to acces of all this datalogs on S7 1200Webserver (save in PLC and SD together) I would like to have a grah production datalog in progress or to can view a old save one. How can i do it ??? Thanks !! |
10/4/2011 5:53 PM | |
Joined: 9/9/2011 Last visit: 4/18/2024 Posts: 102 Rating: (3) |
Hello i would like to directly see my datalog in graphic mode , PHP ... like this : http://www.journaldunet.com/developpeur/tutoriel/php/011121php_jpgraph.shtml is it possible ? |
10/5/2011 12:27 PM | |
Joined: 9/9/2011 Last visit: 4/18/2024 Posts: 102 Rating: (3) |
Ok but if i put a wifi router on the machine, if i would like to check graph on a phone or a tablet it can be usefull. |