4/28/2016 7:08 AM | |
Joined: 11/21/2007 Last visit: 8/12/2024 Posts: 2325 Rating: (308) |
Hello pages.If you do not have a memory card installed, these blocks take up internal load memory space, which is limited according to your CPU model. S7-1200 -A maximum of 30 active HTTP connections. S7-1500–Can be allocated in CPU Communication properties out of the Total upto 256 ( Of the max no of connections ) that the CPU can handle Also be aware that page performance can be affected by the number of active connections. |
Last edited by: Navnag at: 4/28/2016 7:10:02 AMLast edited by: Navnag at: 5/4/2016 5:53:49 PMThere is no such thing as the last bug in a program |
|
This contribution was helpful to4 thankful Users |
5/5/2016 5:21 AM | |
Joined: 11/21/2007 Last visit: 8/12/2024 Posts: 2325 Rating: (308) |
What is a Persistent connection : HTTP persistent connection |
There is no such thing as the last bug in a program |
|
This contribution was helpful to2 thankful Users |
Follow us on