11/17/2008 11:17 PM | |
Posts: 5822 Rating: (412)
|
Dear Cali, well, you know that it is nearly impossible to say that off hand. Actually you should check first of all if a Channel on the 2.4 GHz band is available in the area you want to communicate at. |
Last edited by: J_Bell at: 11/18/2008 10:40 AM |
|
11/18/2008 12:16 AM | |
Posts: 264 Rating: (59) |
Hello Cali, J_Bell is right, it´s not that easy to advise you something in the distance. But perhaps the Sinema Tool could help you: https://mall.automation.siemens.com/AT/guest/index.asp?aktprim=0&nodeID=10034462&lang=de&foldersopen=-4294-4284-4059-4058-1-4297-4298-&jumpto=4298 https://www.automation.siemens.com/net/html_76/produkte/sinema.htm It´s also available as demo, but i didn´t find it now rapid.. I used Scalance W7800 and 6GK5795-6DN00-0AA6 to bridge a distance about 80-90 meters. You could also use 6GK5793-8DR00-0AB6. But that oneonly works with 5GHz.. best regards... |
Follow us on