1/24/2019 9:59 AM | |
Joined: 6/23/2017 Last visit: 9/19/2024 Posts: 9 Rating: (0) |
Hellow, Please, what the corresponding S7 modules for the following S5 Signal Modules : 6ES5103-8MA03 6ES5428-8MA13 6ES5466-8MC11 6ES5470-8MA12 6ES8464-8ME11 6ES5421-8MA12 6ES5452-8MR11 ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 1/24/2019 12:54:56 PMNew subject after splitting |
|
1/24/2019 4:26 PM | |
Joined: 6/23/2017 Last visit: 9/19/2024 Posts: 9 Rating: (0) |
Thank you =D |
2/3/2019 9:23 AM | |
Joined: 6/23/2017 Last visit: 9/19/2024 Posts: 9 Rating: (0) |
Hello, Please What is the equivent of HMI OP5 Ref: 6AV3505-1FB01 |
2/3/2019 2:15 PM | |
Joined: 5/6/2010 Last visit: 9/2/2024 Posts: 1978 Rating: (276) |
Hello shiki, a exactly equivalent is not available. If you need only basic functions then can you use a Basic-Panel 2nd generation. For more information please look at his link: https://new.siemens.com/global/en/products/automation/simatic-hmi/panels.html Hope this is helpful. regards |
This contribution was helpful to1 thankful Users |
2/3/2019 5:07 PM | |
Joined: 9/27/2006 Last visit: 9/20/2024 Posts: 12282 Rating: (2684) |
Hello shiki; I would only add 2 points to CaOd's important information in his post. First, the OP 5 was text-based operator panel, with only messages and alarms available for the control and diagnostics of the machine. If your intention is to use basically the same functionalities with your new panel (there is a lot more that can be done with the modern graphic panels, such as screens, trends, archives...) , this application example could help. Configuration of Messages and Alarms in WinCC (TIA Portal) https://support.industry.siemens.com/cs/ww/en/view/62121503 Second, if you are programming a S7-300 CPU, you can now choose between 2 programming softwares: Step 7 classic (v5.6, now, for Windows 10 compatibility) or TIA Portal Step 7 Professional (now at v15.1, for a s7-300 PLC). If you choose Step 7 classic you should take a ;look at the following video showing the steps to connect a Step 7 classic program for the PLC and WinCC TIA portal for your HMI. Combined configuration with WinCC (TIA Portal) and STEP 7 V5.x (Video) https://support.industry.siemens.com/cs/ww/en/view/73502293 Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 2/3/2019 5:10:41 PM |
|
This contribution was helpful to1 thankful Users |
Follow us on