Industry Online Support
Technical Forum
6/19/2014 2:33 PM | |
Posts: 767 Rating: (69) |
Hello Strongs, The main descriptions of difference can be viewed by product release postings such as below links. SINAMICS V60: https://support.automation.siemens.com/WW/llisapi.dll?func=cslib.csinfo&objid=52681667&nodeid0=52681667&treeLang=en&lang=en&extranet=standard&viewreg=WW&u=NDAwMDAxNwAA&siteID=cseus SINAMICS V90: https://support.automation.siemens.com/WW/llisapi.dll?func=cslib.csinfo&nodeid0=52681667&lang=en&siteid=cseus&aktprim=0&extranet=standard&viewreg=WW&objid=78870735&treeLang=en Best Regards, Deputy |
6/19/2014 4:50 PM | |
Posts: 5225 Rating: (1185) |
Thanks Deputy, I was wondering about the same question and found the answer within the "Getting Started" documents. V60 The amplifier only. It is a "dumb" drive that needs an inedxing pulse much like most stepper motor amplifiers needs an indexer. Open positioning can be done by a PLC such as the S7-1200. V90 A positioning drive. It can handle positioning, torque control and speed control. It can be preprogrammed as if a VSD and more. It only needs commands to be triggered by a button / PLC. Did I miss something? w |
This contribution was helpful to2 thankful Users |
Follow us on