7/3/2021 11:39 AM | |
Joined: 12/20/2012 Last visit: 8/4/2024 Posts: 57 Rating: (0) |
Hello Christoph, What are the hardware differences between S7-1515 and s7-1515T? independent axis control?speed?cycle time? I know it has 1500T is larger memory. Does running a control program take the same amount of time for both? thanks ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 07/05/2021 09:39:42New subject after splitting |
|
7/5/2021 9:58 AM | |
Joined: 3/2/2016 Last visit: 5/29/2024 Posts: 72 Rating: (14) |
Hello KianParax, The big difference between the two is with respect to the use of motion control. You can find the main differences in this link: https://support.industry.siemens.com/cs/ww/en/view/59191792/141313721227 |
7/19/2021 10:18 AM | |
Joined: 3/5/2014 Last visit: 8/5/2022 Posts: 5521 Rating: (1054)
|
hi Kian Parax, yes, according to this manual the times aber the same: SIMATIC S7-1500, S7-1500R/H, ET 200SP, ET 200pro Cycle and response timeshope this helps, regards, |
FCK WAR! |
|
11/19/2022 6:21 PM | |
Joined: 9/27/2006 Last visit: 9/19/2024 Posts: 12282 Rating: (2684) |
Hello KianParax; He are the CPU processing times for the S7-1515-2AM02: They are take from the manual attached below, in section 5, Technical Specifications. You should be able to locate all the information you are looking for in these pages. Hope this helps, Daniel Chartier Attachments71500_cpu1515_2_pn_manual_en-US_en-US.pdf (503 Downloads) |
Last edited by: dchartier at: 11/19/2022 18:23:50 |
|
Follow us on