5/10/2021 9:54 AM | |
Posts: 1 Rating: (0) |
Dear ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 05/10/2021 14:15:32New subject after splitting |
|
5/11/2021 4:49 PM | |
Joined: 10/11/2006 Last visit: 9/18/2024 Posts: 5906 Rating: (804)
|
Hello, you can find the meaning of the LED indications in the corresponding operating instruction manual. If the safe LED is blinking slowly one or more safety functions are active and error-free. So check the selection of your safety integrated functions and make sure that the communication is running in case you are using PROFIsafe. Check the drive for active errors or warnings which could indicate a missing communication. of the drive. When using safety integrated extended functions the drive could trigger an internal STO by itself when i.e. SLS is active but the drive isn`t started within 5 seconds. This is caused by the sensorless safe motion monitoring functions and is described in the following application example. https://support.industry.siemens.com/cs/ww/en/view/82526133 |
With best regards, |
|
This contribution was helpful to1 thankful Users |
Follow us on