6/24/2011 6:27 AM | |
Posts: 259 Rating: (5) |
Hi, If i must be onest i don't understand you very well.... Could you explain what exactly happend... With regards, makaveli |
6/24/2011 4:40 PM | |
Posts: 12 Rating: (0) |
Dear Makaveli: I have to extract the plate MMC of a Sinumerik 840C, there get lost the information TEA1, TEA2, TEA3, IKA, etc Best Regards |
6/27/2011 5:15 PM | |
Posts: 12 Rating: (0) |
Dear Ekalavya: I always thought that data (TEA1, TEA2, TEA3, TEA4, IKA, etc.) is stored in the placa NCK and maintenance of data is through the battery of NCK 9Vdc plate, so I thought that if removes only the MMC board to make a Ghost the HD externally to the machine. I considered reinstalling the same plate with the same HD MMC not affect anything was gonna start the machine, which tells me Ekalavya, I changed everything I thought for the maintenance DATA 840c. Regards Gustavo AttachmentDatos 840C.pdf (195 Downloads) |
7/24/2011 5:35 PM | |
Joined: 7/13/2008 Last visit: 8/23/2024 Posts: 107 Rating: (9) |
Only tea2 needs loaded when the mmc is removed on 840c |
Follow us on