5/15/2018 9:32 AM | |
Joined: 5/12/2006 Last visit: 5/2/2024 Posts: 22243 Rating: (2983) |
Hello, ET200SP https://w3.siemens.com/mcms/distributed-io/en/ip20-systems/et-200sp/Pages/default2.aspx ET200S https://w3.siemens.com/mcms/distributed-io/en/ip20-systems/et200s/Pages/Default.aspx The ET200S is the older decentral I/O System which is successed by ET200SP, for a new machine you should use the ET200SP. What you mean with Interfacing PLC and Remote IO? The Remote IO have a Interfacemodule(IM) which is connected to the PLC. This can be PROFIBUS or PROFINET. Regards Christoph |
This contribution was helpful to2 thankful Users |
5/15/2018 10:32 AM | |
Joined: 8/31/2005 Last visit: 4/26/2024 Posts: 2197 Rating: (326) |
The ET 200SP is the actual system. You can select a PROFINET (recommended) or PROFIBUS Head module and then add IO modules. Use the Mall to get an overview: https://mall.industry.siemens.com/goos/WelcomePage.aspx?language=en Have a look on the configurators just below the Product-tree on the left. Under Automation-Technology you can find the SIMATIC Selection Tool (Cloud):
|
|
|
This contribution was helpful to1 thankful Users |
Follow us on