8/16/2021 9:53 AM | |
Posts: 198 Rating: (60) |
Hello Zankkar, PG/PC mode (default) is mainly used under the cases of project level engineering, diagnostics and maintenance purposes. Configured mode is usually used for OCM in stations which is independent of a STEP7 project, for an automation system networked with controllers. The need/applications for PG or configured mode is further explained in this link: https://support.industry.siemens.com/cs/mdm/109488960?c=64540355083&pnid=15247&lc=en-EG There is not a lot of difference in the configuring the two modes when it comes to Engineering station or HMI servers. In case of HMI stations, the additional step of specifying the access points for the applications exists. You can use the manual below for further detailed explaination: https://support.industry.siemens.com/cs/de/de/view/77377601 Hope this helps |
Last edited by: Jen_Moderator at: 08/16/2021 12:10:27Optimized link. |
|
This contribution was helpful to1 thankful Users |
8/17/2021 7:46 AM | |
Joined: 2/7/2020 Last visit: 1/10/2024 Posts: 101 Rating: (0) |
Thank you for response.. So as I understand, ES: PG mode OS: Initially PG mode & then configure mode from Simatic manager Client: Initially PG mode & then configure mode from Simatic manager Tag server: Initially PG mode & then configure mode from Simatic manager please correct me if i am wrong.
|
Follow us on