10/7/2020 5:05 PM | |
Joined: 12/12/2016 Last visit: 1/15/2021 Posts: 538 Rating:
|
Hello, The advanced and the basic IOT use different chips for the serial interface. The reason is a difference in the internal circuit due to the additional emmc on the advanced version. So while the X30 COM is acessible over /dev/ttyS2 on the Basic version, on the advanced it is /dev/ttyUSB0 The setup and hold times are only configurable on the advanced version, probably because its not part of the SoC. |
10/12/2020 9:25 AM | |
Joined: 4/28/2015 Last visit: 10/12/2020 Posts: 9 Rating:
|
Hi Fe_lipe, Should it be /dev/ttyUSB1? per my test, I have to use /dev/ttyUSB1 instead of USB0 for IOT2050 Advance.
|
Follow us on