Industry Online Support
Technical Forum
2/18/2011 9:52 AM | |
Posts: 65 Rating: (0) |
hello sir, i need to know about working of SMART MCC.i searched abt it in the net and i could not find any information. |
2/20/2011 6:51 AM | |
Posts: 1 Rating: (0) |
"SMATRT MCCs" (also called Intelligent MCCs) are MCCs based on products like SIMOCODE from Siemens. i.e. the MCC feeder has a small controller (SIMOCODE)fitted insideto which all the field signals are connected. The SIMOCODEcan be programmed to handlevarious feeder schemes like DOL/RDOL/STAR-DELTA. TheSIMOCODE also gets connected to a CT module which provides it with the current information for handling the overload functions etc. The SIMOCODE is provided with a communication interface (PROFIBUS DP SLAVE) which can be used for connected to the PLC for monitoring and control. For more information please lookup www.siemens.com/simocode Cheers! |
This contribution was helpful to1 thankful Users |
Follow us on