10/7/2020 10:17 AM | |
Joined: 9/30/2016 Last visit: 4/5/2024 Posts: 910 Rating: (6) |
Thank you for answering again PISCEAN 2010, Please look at the attached screenshots too. I would be happy to attach the starter program if I knew how to export the program for that particular drive. In our Simatic Manager the all the drives progamming and the WinCC 7.4 programming is included apart from the PLC logic. How do I export the Starter program for drive one so that I can attach it?
AttachmentFD 1 RPM A.zip (595 Downloads) |
10/7/2020 11:28 AM | |
Joined: 9/30/2016 Last visit: 4/5/2024 Posts: 910 Rating: (6) |
Thank you again for answering. Please also see the attached screenshots. Yes - only one motor is connected to the drive. (Is MDS drive datasets for each motor?) Here are the values for drive1: p50100 1595.0 A p50101 400 V p50102 11.20 A p40103 0.00 A p50104 5000 rpm p50105 0.1 A p50106 5000 rpm p50107 0.1 A p50108 5000 rpm p60109 Could not be found in the expert list? p2000 1500.00 rpm p2001 1000 Vrms p2002 1600.00 Arms p2003 1000.00 Nm
AttachmentFD 1 RPM B.zip (525 Downloads) |
10/9/2020 10:25 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (872) |
Hello, Please provide below information. p50083, p50609, p0433, p0432. |
10/9/2020 12:40 PM | |
Joined: 9/30/2016 Last visit: 4/5/2024 Posts: 910 Rating: (6) |
Hi PISCEAN 2010, Thank you for answering. Please also see the attached screenshots
p50083 [2] Incr encoder p50609 0 p0433 "No hits have been found" p0432 "No hits have been found"
AttachmentFD 1 RPM C.zip (547 Downloads) |
10/13/2020 10:48 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (872) |
What is value in p922? i.e. telegram type selection in CU & drive? |
Follow us on