5/21/2018 6:59 AM | |
Posts: 3 Rating: (0) |
Wat is the equivalent replacement of the following keyence PLC to siemens. kv7500 kv-c32tc kv-c32xc ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 5/22/2018 7:46:41 AMNew subject after splitting |
|
6/13/2018 10:58 AM | |
Joined: 6/1/2006 Last visit: 8/7/2024 Posts: 129 Rating: (14) |
Hello reichfue1234567890, I have to agree with Duris_I. This question is not simple to answer. Various data have to be considered, when crossing the hardware over to another vendor. Performance: 0.96ns = 0.00096µs per Basic instruction for the Keyence. Here we are matching it up with a S7-1518. Memory: 64MB is stated. How much of that is usable for the program and more important how much has been used? The 1500k steps indicates an average size per step of 44 bytes per step. On could estimate that the 20MB of the 1518 are sufficient. The most important part is the application behind that question. Siemens offers a Conversion Service, which can look closer into the details and can help you finding an appropriate match with all that in mind. Ask your Siemens contact for a Conversion Support. |