9/25/2019 3:35 PM | |
Joined: 11/13/2018 Last visit: 2/26/2023 Posts: 1 Rating: (0) |
Hi DenisMor, i have the same configuration of simotion training case: -CU->D425 -Smart Line Module: 6SL3130-6AE15-0AA0 - Double Axis motor module: 6SL3120-2TE13-0AA3 -Motor A: 1FK7022-5AK7-1LG3 -Motor B: 1FK7022-5AK7-1AG3 I would like to use this configuration with a 220V home line, but i dont' understand what is the tools that i have to connect between 220V output line and the smart module. Can you help me please? ------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 09/26/2019 07:29:12New subject after splitting |
|
Follow us on