3/10/2010 5:20 PM | |
Posts: 5822 Rating: (411)
|
Dear Felipe, I guess you have two of these: IF 963 you may surely order these directly by SIEMENS. Do you have a local contact? Best regards J_Bell |
3/11/2010 4:32 PM | |
Posts: 4 Rating: (0) |
Thank for reply J_Bell Yes that's the module is installed. What i need is the isa card to communicate between IF963-TTY and a PC Do you think this card is going to work? http://www.advantech.com/products/PCL-741/mod_1-2MLI2L.aspx Any comment would be helpful. Thank you |
4/13/2010 8:59 PM | |
Posts: 4 Rating: (0) |
Thank you for asking. I can not figure out yet. People at Advantech couldn't help with this. So I am still looking . I tried with a metrabyte multi protocol card. Without luck. http://cgi.ebay.ca/Keithley-Metrabyte-COM-422-PC7652-14163-Rev-C1-ISA-Card_W0QQitemZ130232538814QQcmdZViewItemQQptZLH_DefaultDomain_0?hash=item1e5276d6be Some ideas?? Thank you. Felipe |
4/15/2010 3:14 PM | |
Posts: 5822 Rating: (411)
|
Dear Felipe, I am sorry that it did not work with the other card too. I found some vendors on the net that supported TTY cards, also for USB, to be used with SIMATIC S5. I think such solutions should also work with you in this case. AttachmentCP441_TTY_EXZ.pdf (64 Downloads) |
Follow us on