5/18/2013 3:51 PM | |
Joined: 1/28/2009 Last visit: 4/1/2024 Posts: 6836 Rating: (1359) |
Hello again, You did not check the "DB Pointer" First of all I strongly recommend to read the following FAQ: STEP 7 -- Creating S7 programs -- Indirect Addressing DW#16#84000040 stands for DBW8 and DW#16#84000010 for DBW2.I mentioned before, it does not matter. Best regards Hamid Hosseini |
5/19/2013 2:40 AM | |
Posts: 8 Rating: (0) |
ok thx i start to get it theDB pointer is 6 bytes long so we jump the first two bytes to get the area pointer stored in the last 4 bytes SO forANY pointer it is 10 bytes long and the area pointer is stored in the last 4 bytes so i need to jump the first 6 bytes... is it right or iam wrong ??!!! I try to simulate it but failed |
5/22/2013 8:46 AM | |
Posts: 8 Rating: (0) |
finally it is working |
Follow us on