12/20/2015 1:55 AM | |
Joined: 1/7/2006 Last visit: 11/17/2023 Posts: 2705 Rating: (318) |
Dear Frank, IMAP is consisting from two parts, the part that is used with STEP7 together won't give a real IMAP link anywhere. It are the interfaces of the blocks that are given with special communication the possibility to make blocks that are containing a whole CPU or even different parts of a CPU in IMAP. SIMATIC iMap STEP 7 AddOn Creating PROFINET Components Service Pack 3 for SIMATIC iMap V3.0 Normally there is a icon placed on the desktop that you could start, please consider the Windows versions from the SP3 above where IMAP works with.... this last update is from 2011.
Getting Started with SIMATIC iMap Configuring Plants in SIMATIC iMap As you might find out, the handbooks are from around 2008/2009.... |
Last edited by: Late at: 12/20/2015 1:59:16 AMI hope that the answer will help, if you have still questions, don't hesitate to ask me. |
|
Follow us on