3/10/2015 6:55 PM | |
Joined: 4/5/2006 Last visit: 8/13/2023 Posts: 642 Rating: (131) |
Hello, the data from the CP you can't use - you only can "translate" the parameters to the new S7-card. Which function has the CP in your configuration? Regards André Räppel --------------------------------------------------------------------------------- www.raeppel.de work faster with innovative PLC-Tools |
3/10/2015 10:18 PM | |
Joined: 9/27/2006 Last visit: 5/10/2024 Posts: 12257 Rating: (2666) |
Hello Mr. Cube; As André has already explained, you simply have to rebuild your netwoprk withj a CP 343-1 or CP 443-1. You have tio determine what Equipment that was connected to your CP 1430, you want to maintain (if any) and see what functions exist in the s7 ethernet CPs that will allow you to do so. If you are using all new Equipment, simply select the type of connection and fnctions will fit your new requirements. Here is how the S5 to S7 manual discusses the transition to an S7 CP 343-1:
SIMATIC STEP 7 V5.5 From S5 to S7
This is the link to the CP 343-1 manual that will show you how you can setup S7 connections or ISO-on TCP connections with newer partners, or ISO transport layer functions with your older Equipment. Hope this helps, Daniel Chartier
|
Follow us on