1/16/2012 1:48 PM | |
Posts: 376 Rating: (57)
|
Hello ShiRaPatil, as attachment I send you apdf-file. In this file you find information about the connector cable PG7xx to S5-150 (AS511 interface module). I think you can use this cable between Field-PG and S5-150S/AS511 interface. The AS511 interface module has a 25 pin sub D connector. Who has still another suggestion? Best Regards Azteke0110 Attachmentcable_PG_to_AS511_Interface_modul.pdf (379 Downloads) |
1/16/2012 4:10 PM | |
Posts: 140 Rating: (1) |
Dear Sir Thanks for reply, man time I was searching for this issue and found one adopter cable to be used with my standard S5 cable ,but it is for CP525. will it work for CP524 also? Please suggest , attached cable adopter . Best regards, AttachmentS5_PG7xx_Cable_Adaptor_CP525.pdf (313 Downloads) |
1/18/2012 3:51 PM | |
Posts: 140 Rating: (1) |
Dear BeeVee, Can I have suggestion please ? Regards, |
1/19/2012 5:11 AM | |
Joined: 10/7/2005 Last visit: 5/9/2024 Posts: 3005 Rating: (1047)
|
Hello ShiRaPatil there seems to be some confusion here, so let's see if we can shed some light on the issue: Scenario 1: Online access to the S5 program What you need is an AS511 module (part number: 6ES5511-5AA12) in the 150 rack. This card is tobe placed in the 9th Slot from the left (Slot "69"), and you can find the PIN layout for its AS 511 portHERE(which is the smae as Azteke0110's advise). To be clear, you can NOT use the CP524 (nor a CP525 or any other CP) as an "access point" for online access to your S5 program. Question is: Do you have an AS511 module in your rack? Scenario 2: Online access to CP524 program I'm afraid to say this is not possible. Only the second interface of a CP525 allows this and below are the links to themanuals which contain all the relevant info on the cards as well as its programming: COM 525 Programming Package for the Communication Processors CP 524 and CP525 (S5-DOS) Volume 1/2 COM 525 Programming Package for the Communication Processors CP 524 and CP525 (S5-DOS) Volume 2/2 Last but not least, possibly the best advise I can give you is to upgrade your system to an S7 (and then throw the ancient 150 system into the bin). I hope this helps |
Last edited by: fritz at: 1/19/2012 5:13 AMCheers |
|
Follow us on