2/6/2017 9:47 AM | |
Posts: 5 Rating: (0) |
Dear Experts From external influence is out of order module TM31 6SL3055-0AA00-3AA0 (works in conjunction with SINAMICS G150). It was bought a TM31 module 6SL3055-0AA00-3AA1, the seller claimed that it is full analog, but after replacing SINAMICS G150 is not working. Module TM31 6SL3055-0AA00-3AA0 taken with other SINAMICS G150 works. What you need to do to SINAMICS G150 worked with a TM31 module 6SL3055-0AA00-3AA1? Sorry, the translation is made on the computer Thanks & Regards. Vadim ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 2/16/2017 5:13:15 PMNew subject after splitting |
|
2/6/2017 9:59 AM | |
Joined: 5/12/2006 Last visit: 9/20/2024 Posts: 22365 Rating: (3011)
|
Hello, check which faults/errors are present after change to the new TM31.
Christoph |
2/16/2017 11:24 AM | |
Posts: 5 Rating: (0) |
Hello, F01352 Regards, Vadim |
2/16/2017 11:31 AM | |
Joined: 5/12/2006 Last visit: 9/20/2024 Posts: 22365 Rating: (3011)
|
Hi, do you have the Alarmtext? I cant find the Alarmnumber f01352 in my list.
Christoph |
2/16/2017 12:27 PM | |
Posts: 5 Rating: (0) |
There is only hard copy Yandex translate F01352 Topology: it is impossible to determine the actual topology Reaction: NONE Cause: unable to determine the actual topology. - Lack of memory. - Internal access settings incorrect. - Unknown component ID. Measures: - to Reduce the number of data sets or drives. - Turn off and turn on the power. Acknowledge: Power On. Google translator F01352 Topology: Unable to determine actual topology Reaction: NONE Reason: Unable to determine actual topology. - Insufficient memory. - Internal access to the parameters is invalid. - Unknown component ID. Measures: - Reduce the number of data sets or drives. - Turn off and turn on the power. Acknowledgment: Power On. scan copy in the attachment Regards Vadim AttachmentF01352-.pdf (112 Downloads) |
Last edited by: Vanikk at: 2/16/2017 12:30:13 PMLast edited by: Vanikk at: 2/16/2017 1:27:39 PM |
|
2/16/2017 12:50 PM | |
Posts: 5 Rating: (0) |
"Is it F01325 or F01352?" F01352 See message below Regards Vadim |
Last edited by: Vanikk at: 2/16/2017 12:52:48 PMLast edited by: Vanikk at: 2/16/2017 12:57:13 PM |
|
2/21/2017 10:00 AM | |
Posts: 5 Rating: (0) |
Hi, Today, there is another fault after switching on the drive. See the attached file Regards, Vadim AttachmentNew fault.pdf (133 Downloads) |
Follow us on