4/1/2020 6:37 PM | |
Posts: 3 Rating: (0) |
Hello, We have NCU 720.3 version V4.8 SP05 HF04 I use starter version V5.1.1.2 and have SSP 5.2 and 5.1 installed. When connecting via starter I see two nodes but they are marked with ? and I get the remark to install the simanics (see attachment) Any idea what can be wrong? Thx Thierry ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 04/02/2020 05:43:19New subject after splitting |
|
4/1/2020 7:14 PM | |
Posts: 3 Rating: (0) |
Hello, it is a real NCU, SINUMERIK 840D SL NCU 720.3B PN WITH PLC 317-3 PN/DP in attachment more info about the nodes |
4/1/2020 7:19 PM | |
Joined: 5/12/2006 Last visit: 9/18/2024 Posts: 22364 Rating: (3011) |
and if you follow the link to the ssp can ou download and install it? |
4/2/2020 5:46 AM | |
Joined: 5/12/2006 Last visit: 9/18/2024 Posts: 22364 Rating: (3011) |
Hi, if you really have a NCU with FW V4.8 you need SSP V4.8, not 5.2 not 5.1. Regards Christoph |
Follow us on