8/12/2017 5:02 PM | |
Posts: 5 Rating: (0) |
Hi Everyone! I Have an OP77A. I am Transferring project file to that op by USB-PPI cable with transfer setting channel 1: serial Enable and Channel 2: MPI Disable. My project contains 4 files, all 4 files are transferred, erasing flash memory is completed but when copy files to flash memory then an error occurred and transfer interrupted. Anybody Please Help.... I think my project has the setting MPI/Profibus: Enable and Serial: Disable and in the last step when these settings are transferred to flash memory then data transfer through serial USB-PPI is also interrupted. Any Solution???? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 8/14/2017 7:44:15 AMNew subject after splitting |
|
8/14/2017 8:38 AM | |
Joined: 4/24/2006 Last visit: 4/22/2024 Posts: 8611 Rating: (1147)
|
Hello Abuabkar, Can you explain, which error you get? Which software are you using? Version? Best regards, Wizard |
8/16/2017 3:37 PM | |
Posts: 5 Rating: (0) |
Only Text Comes up "an error occurred during transferring project". I am Using simatic prosave. |
Follow us on