9/16/2018 6:47 AM | |
Joined: 1/1/2017 Last visit: 7/22/2024 Posts: 331 Rating: (11) |
Dear All, Presently I'm facing the same situation....I've edited & added some existing functions in STL in the OB1 block & have to downloaded it... Now when I'm going online the block is not showing running status & the logic is not working....All sorts of Block, FB, Fccalling has been checked in OB1 but it's not working.... Actually I don't know how to compile the SCL program so that it can be edited in STL version...Can you provide me some manual or link that how to sort out with this issue... I'll be very grateful to the team by on then.... Regards OmKris ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 9/17/2018 8:24:46 AMNew subject after splitting |
|
9/21/2018 6:42 PM | |
Joined: 1/1/2017 Last visit: 7/22/2024 Posts: 331 Rating: (11) |
Hello! Thank you Piotr. The quote is really notifying! Yes there are 05 NW in the OB1. After that I've transferred them to OB35. Interestingly only the first NW is running but not the rest 04. I'm simply confused that whenever I'm calling the FB45 of Siwarex Library from that NW till the end one are becoming non responsive! I'm really confused. If a Block is called in Cycle then how the first NW is not ending it's cyclic calling because the next NW's are not called simultaneously! I'm attaching the backup for checking. Please guide me to the solution. Thanks Regards OmKris Attachment1224_LOADTEST_TRIAL_19092018.zip (71 Downloads) |
Follow us on