8/30/2021 7:55 AM | |
Joined: 12/18/2014 Last visit: 9/21/2024 Posts: 33810 Rating: (4201)
|
Import of a technical question via PM from the Nimspatel007. Hi, i am created program logo plc. I put network input and network analog input in program. When i command 0 or 1 to network input V0.0, a network analog input VW0 value Change automatically. Why this happened? Please help |
8/30/2021 7:56 AM | |
Joined: 12/18/2014 Last visit: 9/21/2024 Posts: 33810 Rating: (4201)
|
Bit V0.0 is part of VW0. Bits V0.0 to V0.7 result in VB0. Bits V1.0 to V1.7 result in VB1. VB0 and VB1 from the VW0.
AttachmentLOGO! Bit, Byte, Word and DWord.pdf (266 Downloads) |
Follow us on