4/1/2010 8:35 AM | |
Joined: 11/15/2009 Last visit: 2/5/2024 Posts: 380 Rating: (47) |
Hello Sam. |
4/1/2010 9:03 AM | |
Posts: 63 Rating: (0) |
Hello JOTST, For above link... "No root node found for tree 'cs:_::22352509:4000002_WW:4000003_WW:_:en'." Plz provide healthy link......... |
4/1/2010 10:01 AM | |
Joined: 4/5/2006 Last visit: 3/13/2024 Posts: 917 Rating: (63) |
Hi Sam,
not to understand the question. Do you means to buy the RACK, PS, CPU, CP in separate way? When you buy by BOUNDLE order code using PCS7 catalogue you don't have any problem (and cheaper than buy modules separated) If you need to buy in separate way, for example when you have to uograde system, have a look in "PCS7 Released Modules" as well as JOST mentioned, located in PCS7 documentation, or follow this link Which modules and their firmware versions are released for PCS 7 and how can you upgrade them? hope can help regards |
4/1/2010 12:08 PM | |
Joined: 4/5/2006 Last visit: 3/13/2024 Posts: 917 Rating: (63) |
Hi Sam, you have to ask your local sales manager, or go to Siemens web portal support.automation.siemens.com http://support.automation.siemens.com/WW/llisapi.dll?aktprim=99&lang=en&referer=%2fWW%2f&func=cslib.csinfo2&siteid=cseus&extranet=standard&viewreg=WW then select, from the top, "ProductSupport" then select, from the right, "Catalogue and ordering system online" and "Show catalog/order" all Siemens catalogue weill be displayed, look for "Process Control" section from left select Atomation Technology -> Automation & control system -> Process control system -> Simatic PCS7 only PCS7 catalogues will be displayed and ready to download (if you want) regards |
4/1/2010 12:56 PM | |
Posts: 63 Rating: (0) |
Thank you @massad and @CBo. |
Follow us on