9/7/2011 7:48 AM | |
Joined: 3/21/2006 Last visit: 4/4/2024 Posts: 10228 Rating: (1181) |
Hello, I don't have at the moment Simatic Manager in order to try your modules like a hardware configuration. If there is allowed to put that module seems the configuration is correct. After you will need http://support.automation.siemens.com/WW/view/en/19350076 . When that behavior occured how did you return back the previous healthy state of CPU? Best regards, Hristo Mihalev |
Last edited by: UMENCHO at: 9/7/2011 7:49 AMtypo |
|
9/7/2011 11:02 AM | |
Joined: 12/12/2009 Last visit: 7/17/2022 Posts: 9 Rating: (0) |
Hello Hristo, The bus connector is attached( see in the con_HW.jpg ). When I downloaded the HW config and put the CPU in RUN without the analog card, the SF led is staying ON for 1 second, after that is OFF, I am getting an error in HW Diagnostics(see con_HW.jpg) but the rest of the system is functional. I can get signals from DI...etc. When I clear all the CPU, put the modules without the SM331 I don't have SF on. When I put the SM331 all the LED's are ON.I tested with OB block's that are special for errors. No result. I think that the module is broken. I will try to send back the module to be tested. I will tell you the result. UMENCHO and Marcjan thanks for your support Best regards, Alin.NST |
Follow us on