9/7/2018 12:23 PM | |
Posts: 178 Rating: (5) |
Gents, No idea why I get a question mark ? when inserting an AFP block. Any ideas? Thanks, gbs |
9/7/2018 12:25 PM | |
Posts: 64 Rating: (7) |
Its when the enable signal is connected to signal (it doesn't know if its enabled or not) |
This contribution was helpful to2 thankful Users |
9/7/2018 1:00 PM | |
Posts: 178 Rating: (5) |
How do I get around it as I am using a OpDiL to enable the timer. |
9/7/2018 1:14 PM | |
Posts: 64 Rating: (7) |
I think its just an indicator that the code might not always be called, but it should work fine when EN=1 by signal. |
9/7/2018 10:28 PM | |
Joined: 3/14/2008 Last visit: 4/24/2024 Posts: 2065 Rating: (927)
|
In addition to what K2016 said, when the block is not enabled (EN=0), then a red exclamation mark is shown in the block. |
If I could help you, you can use the RATE button. Thank you. |
|
Follow us on