11/9/2020 3:42 PM | |
Posts: 15 Rating: (0) |
Hellow, It looks like I'm having the same problem as mentionned above. Though I'm not able to fix it. Can annyone help me maybe? I have a real PLC too which i can connect and response correctly at my watch table inputs. But when I open the HMI simulation it tells me "change to operating mode 'online'. I'm not sure how to, but when I try to go online, when I use my ethernetcard ofcourse he doesn't find the HMI at the IP adress. and when I use PLCSIM: not sure if this correct what I'm doing? Maybe there is my problem. But so, I set my PG-/PC interface to S7ONLINE I used the same name for the accespoint in the HMI connection but when simulated i cant get connection with my PLC. Can somebody help me? kind regards I'm using TIA V16 ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 11/10/2020 09:59:36New subject after splitting |
|
11/10/2020 6:20 AM | |
Joined: 9/21/2012 Last visit: 4/26/2024 Posts: 3930 Rating: (444) |
If you have a real PLC, the S7ONLINE should be your network connection, not PLCSIM. |
11/10/2020 8:13 AM | |
Posts: 15 Rating: (0) |
I can connect with the plc it's the HMI i can't get to run |
11/10/2020 8:20 AM | |
Joined: 5/12/2006 Last visit: 4/26/2024 Posts: 22231 Rating: (2980)
|
do exactly what we adviced before change for s7online PLCSIM.tcp to <networkcard>.tcpip |
11/10/2020 8:39 AM | |
Posts: 15 Rating: (0) |
i hope you guys can see the printscreens? because i can't see them but when edit the message they are there |
11/10/2020 9:11 AM | |
Joined: 5/12/2006 Last visit: 4/26/2024 Posts: 22231 Rating: (2980)
|
no screens attached |
11/10/2020 9:43 AM | |
Posts: 15 Rating: (0) |
I think the first prinstscreen is vissable now? But for some reason I can't get the second vissible so I added as an attachement |
11/10/2020 9:51 AM | |
Joined: 5/12/2006 Last visit: 4/26/2024 Posts: 22231 Rating: (2980)
|
the one we see is enough. you select the wrong adapter. in you screen is the <adapter>.iso and not <adapter>.tcpip |
11/10/2020 10:42 AM | |
Posts: 15 Rating: (0) |
Oke changed the TCP/IP one This results in the nxt message see attachement grtz |
Last edited by: Ninjag at: 11/10/2020 10:44:26 |
|
Follow us on