9/28/2017 1:54 AM | |
Posts: 18 Rating: (0) |
I'm also having a project upgrade fail. The log identifies the problem; but, I don't know where to find it in the V13 project, which runs fine. Here's a snippet of the exception text; I've attached text file as the details. Exception "System.ArgumentNullException" during conversion of core object with the name: "Profi_1" and ID: "{1052686-22162}". "Error occurred while converting the object 'Profi_1' of type 'Device' (model type 'Siemens.Simatic.HwConfiguration.Model.DeviceData')" The core object mentioned, 'Profi_1' was a device configured in the project. But it is no longer in the project; I either renamed it or deleted it and added a new one. I've recompiled all hardware and software blocks thinking there is something not getting cleared out. Thanks, ------------------------------------------------------------------------------------------ AttachmentTia13To14_exception.txt (239 Downloads) |
Last edited by: Jen_Moderator at: 9/28/2017 12:58:02 PMNew subject after splitting |
|
Follow us on