7/9/2008 3:43 PM | |
Joined: 4/24/2006 Last visit: 5/13/2024 Posts: 8641 Rating: (1151) |
Dear Begginer, The fifth dipswitch must be set to zero position. See also this faq: http://support.automation.siemens.com/WW/view/en/23787153 Best regards, Wizard |
7/10/2008 8:47 AM | |
Joined: 4/24/2006 Last visit: 5/13/2024 Posts: 8641 Rating: (1151) |
Hello Darius, There are some panels, which you can transfer using a RS232 cable. Have a look at following faq: http://support.automation.siemens.com/WW/view/en/19109408 They are mostly older panels. Because Begginer mentioned an OP73 Micro, I told that it isn't possible with that panel. Sorry if I wasn't clear enough. Best regards, Wizard |
7/10/2008 9:05 AM | |
Joined: 9/28/2005 Last visit: 3/12/2024 Posts: 2957 Rating: (242) |
Hi, Thats ok, I just wanted to make it clearer |
Best regards, |
|
7/10/2008 10:59 AM | |
Posts: 112 Rating: (0) |
Hi, One more question, can op73micro can communicate to s7314c? |
7/10/2008 11:39 AM | |
Joined: 4/24/2006 Last visit: 5/13/2024 Posts: 8641 Rating: (1151) |
Hello Begginer, You have RS232/MPI ?
Well this article is a RS232 PC/PPI multimaster cable. You have to choose in WinCC flexible, transfer settings -> RS232 It is not possible to connect OP73 Micro to S7-300 CPU. Only S7-200. See faq: http://support.automation.siemens.com/WW/view/en/21120013 Best regards, Wizard |
Follow us on