1/8/2020 7:35 AM | |
Posts: 2 Rating: (0) |
I have DI 256, DO 128, AI 56, AO 56 I want to use S71200 series PLC. Which model i will select. CPU1215C or CPU 1217C Please suggest Shruti.... ------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 01/09/2020 16:49:33New subject after splitting |
|
1/12/2020 7:53 AM | |
Posts: 2 Rating: (0) |
Yes. Because of cost effective solution S71200 I am considering. Using 1217C with ET200S IO can I configure? |
1/12/2020 9:57 AM | |
Joined: 5/6/2010 Last visit: 4/20/2024 Posts: 1963 Rating: (272) |
Hello, a 1200 is possible but it's easier to use a ET200SPCPU, e.g. 1512. Then can you directly use all the ET200SP-modules. To configure your system you can use the TIA-Selection Tool regards |
Last edited by: CaOd at: 01/12/2020 14:49:50 |
|