7/18/2013 5:43 PM | |
Joined: 1/3/2006 Last visit: 2/19/2024 Posts: 726 Rating: (71) |
Hi Please refer to page 37 ofTHISmanual. It gives you the meaning of various LED combination. As per this manual "The interface module is not configured or isconfigured incorrectly. No data exchange is taking place between the DP master and the interface module". So check whether the profibus address of IM (DIP switch) is same as that of hardware configuration. Regards Manmeet
|
7/20/2013 11:13 AM | |
Posts: 18 Rating: (1) |
you will found attached file have Dignostic for HWC Dign,,Screen Shot for HW Configuration i tried to check the addresses and change it many time in DIP Switches Physical and in HW Configuration and redwonload but the resuslt was the same,,, and the same in bus connector switches make it ONand OFF depend on the node loacation in network the nodes is show rightly in Accessible nodes for CPU and Two IMswith assigned addresses AttachmentNew Folder.zip (209 Downloads) |
7/20/2013 11:27 AM | |
Posts: 18 Rating: (1) |
yea i used this manual to know the LEDs identification and in the same manual found some Paramters Setting in P-55 in IM , PM, DS and i found in IM paramter items 1- DP interrupt mode DPV 0 default and DPV 1 so i doubt in this paramter should be DPV 1 i'don't know what's mean.. 2 -Operation at preset<>Acutal at configuration this able hotswaping during operation and should be enable i'll check these in site So, from first i doubt in paramter setting |
Follow us on