7/20/2011 12:27 PM | |
Joined: 1/28/2009 Last visit: 4/1/2024 Posts: 6836 Rating: (1359) |
Dear GzStrom Programmable logic controllerSIMATIC S7-300 S7-300 Automation System Module DataSIMATIC S7-300 CPU 31xC and CPU 31x: Technical specifications WinCC: General information or SIMATIC HMI WinCC flexible 2008 ProAgent PLC can provide all range of module you need.You just proide a brief description here and we may suggest you list of module you may need! HMI or SCADA can help you by archiving process values or and providing interface to your machine or process. DI,DO,AI and AO are interfaces to your process. Regards |
7/21/2011 1:43 PM | |
Posts: 2 Rating: (0) |
Well it needs to switch on 2 devices, then receive inputs from sensors for wind speed, temperature, water temperature, pressure and flow rate of the water |
7/21/2011 2:06 PM | |
Joined: 1/28/2009 Last visit: 4/1/2024 Posts: 6836 Rating: (1359) |
Dear GzStrom The 2 devices you want to run,if only on-off status is required Digital Output module is sufficient. Check chapter 4 of this manual for types of analog input modules and tips for connecting. Also check the chapter 6 for different modules and their characteristics! Regards Attachmentanalog overview.pdf (197 Downloads) |
8/31/2011 4:19 PM | |
Joined: 4/22/2010 Last visit: 2/15/2024 Posts: 5697 Rating: (711) |
Just to confirm Umencho : http://support.automation.siemens.com/WW/view/en/40466101 Regards, Marcjan |
Problem solved? |
|
Follow us on