Industry Online Support
Technical Forum
8/29/2014 7:21 PM | |
Posts: 3 Rating: (0) |
saludos tengo que comunicar mi S7-1200 with s7-300 en master / slave, pero en el paso 7 v5.5 NO EXISTE S7-1200 alguien me puede ayudar?
|
9/2/2014 11:14 PM | |
Posts: 5225 Rating: (1185) |
Hi there. It is possible to develop a link between S7-300 and S7-1200 without working in the same design environment. The two communication parteners can have different projects. Ste39 has given a link to show this. The question is rather.. what communication medium is available from the S7-300? If only MPI - then you have a problem. Although (€xpen$ive) converters Something like Profibus, Profinet or Modbus makes it possible. Are there other communication partners (example: ET200 / HMI)? It will also be helpful to know also what type of data needs to be shared. Maybe analog or digital signals can be used instead. With your comments on these text, I am sure there will be more to work with for you. Greetings. w |
9/3/2014 12:56 AM | |
Posts: 3 Rating: (0) |
thanks fot the help the PLC is a 6ES7315-2AG10-0AB0, which has a RS 485 interface(Profibus). the signals thatwill share are only digitals |
9/3/2014 8:19 AM | |
Joined: 1/21/2013 Last visit: 3/19/2024 Posts: 4618 Rating: (705) |
Hello, Wizard wrote: When you want to use Profibus. And the S7-315-2DP is master, then you need the CP1242-5 (Profibus slave communication module)for S7-1200 Here you can download the GSD file, you can import in Step 7 V5.5: Download GSD File CM 1242-5 Try with this and send us the result
|
Last edited by: Ste39 at: 9/3/2014 8:21 AM |
|
9/3/2014 9:52 AM | |
Posts: 5225 Rating: (1185) |
Late add.. [CPU-CPU communication with SIMATIC controllers (compendium)] |
9/3/2014 3:55 PM | |
Joined: 1/21/2013 Last visit: 3/19/2024 Posts: 4618 Rating: (705) |
Hello, Have a look this thread also: how to configure s7-300 and s7.1200 communication through Profibus ... |
Follow us on