11/18/2019 9:23 AM | |
Joined: 9/30/2016 Last visit: 4/5/2024 Posts: 910 Rating: (6) |
Hello Georg, Thank you for answering. It is a single-station with Simatic Net. I have set up autostart by having opened the Auto Start Configuration and browsed to the location of the project. Made the local computer the server and ticked of all 3 options in the highlighted area. Se the attached screenshot when the mentioned setting are located (but not correct in the screenshot since this screenshot was taken of a completely different PC). So you are saying the reason it fails occasionally is that it is too busy at the start time. https://support.industry.siemens.com/cs/ww/en/view/19249315
|
Last edited by: Jen_Moderator at: 11/18/2019 13:47:20Optimized link. |
|
Follow us on