10/19/2020 1:04 PM | |
Joined: 3/19/2015 Last visit: 1/10/2022 Posts: 30 Rating: (1) |
Hello, I think that the FAQ is a bit ... tricky. On the first steps the manual tells to send the program to the S120 disconected from any other DRIVE-CLIq, power the Control Unit CU320-2PN and then send the program from the V14 project. Does this step is necessary if the machine is already running? I don't think so! Why we should send the configuration to the S120? (I am enrolled on one of this migrations, our customer desires a half-hour migration and avoid stop the production). ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 10/19/2020 14:07:23New subject after splitting |
|
10/19/2020 3:37 PM | |
Joined: 7/7/2010 Last visit: 4/25/2024 Posts: 14629 Rating: (2348) |
Is the programming / configuration of the S120 changing? If it is changing, but the hardware connected to the CU320-2 PN is not changing (same motor, same power module and so on), you should be able to make changes in the drive and upload to the PG/PC (after testing and saving RAM->ROM).
|
science guy |
|
This contribution was helpful to1 thankful Users |
Follow us on