4/15/2013 1:25 AM | |
Posts: 41 Rating: (0) |
Dear Colleagues, I have a trouble setting up communication between WinCC V11 SP2 and RTX2010. The WinCC Channel diagnosis says : error 42C2 (Online: The logical device is not defined in the registry.) The winCC project has only one tag namely M0.5 (1Hz clock). also attached the runtime sceenshots for : winCC; Station configurator and RTX 2010. I noticed , in the station configurator; that the staus icon for WinCC Rt and RTX 2010 are greyed .and maybe that this lies behind the communication error. Would you please help as I am Under pressure of project commissioning right now. Best regards Attachmentattachement.zip (392 Downloads) |
4/18/2013 11:01 AM | |
Posts: 3037 Rating: (192)
|
Hello, You can find all communication errors of WinCCin the following file. See "Error codes during connection problems". Tweety AttachmentD:\S7CHNERRORENU.zip (394 Downloads) |
4/22/2013 1:03 PM | |
Posts: 3037 Rating: (192)
|
Hello, You should see in this link if your software works together. With what are SIMATIC WinCC V11 and WinCC V12 compatible? Tweety |
4/23/2013 8:58 PM | |
Posts: 41 Rating: (0) |
Hi Tweety, I already opened a support request and investigation is ongoing. Many Thanks for your support |
Follow us on