5/21/2012 10:22 AM | |
Joined: 9/19/2009 Last visit: 5/11/2024 Posts: 458 Rating: (81) |
Hello Everybody with WinAC RTX (F) and when I tried with TCP Protocol or UDP Protocol, a warning tell me that not is possible as Attachment shows. It is possible? Thanks |
If my answer help you, use the Thanks or Rate Button, It is free of charge :-) |
|
5/21/2012 11:15 AM | |
Joined: 9/22/2010 Last visit: 12/13/2023 Posts: 225 Rating: (28) |
Hello JM76, when you use a CPU with an integrated Profinet Interface or a WinAC RTX, NetPro is not used to setup TCP or UDP connections. NetPro is used for static connections with a CP. But when you use the PN interface of the CPU / of the WinAC, you have to use the communication blocks TSEND, TRCV, TCON and TDISCON. You can find a lot of information about the use of this communication blocks here: http://support.automation.siemens.com/WW/view/en/29737950 Regards Sakura |
This contribution was helpful to1 thankful Users |
5/21/2012 1:19 PM | |
Joined: 9/19/2009 Last visit: 5/11/2024 Posts: 458 Rating: (81) |
|
If my answer help you, use the Thanks or Rate Button, It is free of charge :-) |
|
Follow us on