7/26/2013 1:41 PM | |
Posts: 1530 Rating: (59)
|
Hello armagan, did you already take a look at .../Siemens/WinCC/diagnose, because there you will find diagnose files and for sure there should be an entry for the time your fault ocurred. What happens if you try to start runtime again? Do you have to use reset_wincc.vbs, because some parts of WinCC are hanging, maybe Graphics Runtime (GSCRT)? Do you have any archives in your WinCC Project? If yes, are they still working fine, after problem occured? If not please take a look at this older thread incl. links. Best regards Bizur |
This contribution was helpful to1 thankful Users |
7/29/2013 10:49 AM | |
Posts: 18 Rating: (0) |
Hello Bizur, *I looked the log files, it gives CRTApplication error..(given in the attachment) *I tried to reset wincc but it did not work. *Yes, I use archives,but I suppose they work fine. AttachmentPMDeactivate.zip (312 Downloads) |
7/31/2013 11:58 AM | |
Posts: 1776 Rating: (95)
|
Hi, WinCC V7.0 Sp3 is not released for your operating system. See the compatibility tool https://support.automation.siemens.com/kompatool/pages/main/index.jsf |
7/31/2013 1:07 PM | |
Posts: 18 Rating: (0) |
Hi, I have checked the list that is on the list for WINCC 7.0 SP3, it supports my operating system. I have also update 1 package. However the project was created in 7.0 SP1. I did not find any tool that converts my project to 7.0 SP3 on the link. |
Follow us on