12/18/2016 1:23 PM | |
Joined: 9/8/2016 Last visit: 6/29/2024 Posts: 198 Rating: (10) |
Hi, Quick question - it seems that WinCC make lower quality after import *.png and used it in Graphic Object. What want to achive to have couple of 30x30 pixel graphic and use it in my future faceplate. In attachement you can find example *.pdl called "NewPdl1" and i put there graphic which i draw using wincc tool and imported *.png drawed in vector graphic tool (in my case Inkscape). The sizing is the same but quality is much diffent. Why? It thinh i miss something because it is impossible that my imported picture appear with that low quality in wincc *.pdl. Attachmentforum.zip (149 Downloads) |
12/18/2016 6:20 PM | |
Joined: 3/14/2008 Last visit: 9/20/2024 Posts: 2095 Rating: (936) |
Hi, The way I do it is creating pictures as .EMF format. I create them with Microsoft Powerpoint. Most of the time, I draw my objects in WinCC Graphics Designer, export them as .EMF and import after editing them in powerpoint. No Jpeg or other format... Siemens also create their objects as EMF. |
If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to4 thankful Users |
12/21/2016 8:00 PM | |
Joined: 3/14/2008 Last visit: 9/20/2024 Posts: 2095 Rating: (936) |
Hi SuHu, Glad I could help. Thx for the info on the .svg file. I'm gonna try this sometime |
If I could help you, you can use the RATE button. Thank you. |
|
Follow us on