6/11/2018 12:40 PM | |
Posts: 17 Rating: (0) |
Hello everyone, I was wondering if anyone has faced a graphic issue with the dynamic filling option... currently on our client Siemens IPC , when the dynamic filling is enabled the graphic items start to flicker when the level is not 100% or 0% and when trying this SCADA on our machines it also does the same ... so what is going on here.. Iattached a sample for the tank level and how it affects what ever item in the dynamic filling way. AttachmentDynamic Filling Issue.zip (63 Downloads) |
Follow us on