Industry Online Support
Technical Forum
11/14/2012 11:15 AM | |
Posts: 3037 Rating: (192)
|
Hello MarceloSCS, Yes, you can upgrade this license WinCC V7.0 RT version to a license of WinCC Runtime Professional V11. You can not use this License with WinCC Runtime Advanced. WinCC flexible 2008 -----> WinCC Advanced V11 WinCC V7.0 ------> WinCC Professional V11 Which licenses do you need to upgrade from WinCC flexible 2008 or WinCC V7 to WinCC V11 and in WinCC V11? Tweety |
11/14/2012 11:58 AM | |
Posts: 17 Rating: (0) |
Hi Tweety So, if I install WinCC V7.0 RT in a Computer. I cannotrun projects made from WinCC Advanced V11 without any upgrade? Upgrading the Advanced to Professional, can I made projects to run with WinCC V7.0 RT or I need alsoupgradethe WinCC V7.0 RT? Thank you so much for your answer!! |
11/14/2012 1:10 PM | |
Posts: 3037 Rating: (192)
|
You can notrun a project of WinCC Advanced V11 or WinCC Professional V11 with WinCC V 7.0 RT. You can migrate a WinCC V7.0 project to WinCC Professional V11. Then you can use WinCC Professional V11 RT. The other way from WinCC Professional V11 to WinCC V7.0 is not possible. Service Pack 2 for WinCC V11
You can not Upgrade from WinCC V11 to WinCC V7.0. You need WinCC V7.0 if you use the WinCC V7.0 RT. Tweety |
This contribution was helpful to1 thankful Users |
11/14/2012 3:00 PM | |
Posts: 17 Rating: (0) |
I understood it now! Thank you Tweety |
This contribution was helpful to1 thankful Users |
Follow us on